Ingress Protection: Where and Why It Matters
By Steve Schriber for Mouser Electronics
Electronics are like a grumpy neighbor: Neither can tolerate wet and dirty
contaminants (kids) in their enclosures (yards). The International
Electrotechnical Commission (IEC) has developed a set of Ingress Protection
(IP) ratings that serves as a unified system of designating electronic
enclosure wet and dry contamination resistance. This article discusses why
electronics are particularly averse to contaminants and how contaminants
enter electronic enclosures, as well as discusses IP ratings and examples.
Why Electronics are Contaminant-Averse
Any contaminants entering an electronic enclosure or case can cause damage
ranging from shortened usable life to ultimately rendering the equipment
useless. Dust and dirt entering an electronic enclosure can do harm in any
one of many ways. Dust is capable of accumulating inside the sockets,
ports, and crevices of electronics and circuits. If dust builds up
excessively, bad things can happen: The dust may build up to form an
insulating layer that causes the circuits to overheat. If the dust or dirt
inserts itself between contacting surfaces, poor conductance may occur
creating problems for switches, relays, and connectors. In higher voltage
applications, the dust and dirt may facilitate arcing between line voltage
and ground.
Wetness, aka water, moisture, and humidity are sworn enemies of
electronics, especially with delicate microcircuits. Rugged environments
are where the product is at the mercy of the weather, be it heavy
thunderstorms or light drizzle. Cleaning equipment with simple flowing
water can create problems let alone a high pressure
stream (self-service car washes are an example of electronic enclosure
abuse every time someone chooses to clean under the hood). Even humid
environments can form problematic condensation on internal components. A
device moved from a cold environment to one that is warm and humid may see the formation of moisture
on circuitry. If the power is applied before this condensation can
evaporate, short circuits can cause failure.
Exposure to harsh chemicals, surfactants, or cleaning liquids such as those
used in high-pressure spray cleaning
equipment can have a corrosive, damaging effect on electronics and
circuitry. Copper, aluminum, and silver compounds are particularly
susceptible. Corrosion deteriorates the base metal resulting in diminished
current carrying capacity. The ever-shrinking size of electronic components means there is less conductive mass
to deteriorate and, therefore, increases the vulnerability of failure.
IEC IP Rating System Overview
Not to be confused with the highly recognized Internet Protocol, the IEC IP
standard measures ingress protection and has become increasingly popular as
consumer electronic devices become more mobile with a focus on ruggedness.
The IP designation (or code) is a two-digit number, as in IP67, IP68, and
IP69K:
- The first digit of the IP Code indicates the device's protection level against solid objects.
- The second digit shows how well liquids are kept from the electronic components and circuitry within the enclosure.
As Table 1 shows, solid and liquid protection levels
increase with higher designated ratings.
Table 1:
In IEC IP ratings, solid and liquid protection levels increase with higher
designated ratings.
|
1st Digit
|
Description
|
2nd Digit
|
Description
|
|
0
|
Non-protected
|
0
|
Non-protected
|
|
1
|
Protected against objects >50 mm
|
1
|
Protected against drips
|
|
2
|
Protected against objects >12.5 mm
|
2
|
Protected against drips if the
housing is bent at an angle of 15°
|
|
3
|
Protected against objects >2.5 mm
|
3
|
Protected against spray-water
|
|
4
|
Protected against objects >1.0 mm
|
4
|
Protected against splash-water
|
|
5
|
Dust protected
|
4K
|
Protected against splash water at increased pressure
|
|
6
|
Dust-tight
|
5
|
Protected against jet-water
|
|
|
|
6
|
Protected against strong jet-water
|
|
|
|
6K
|
Protected against strong jet-water at increased pressure
|
|
|
|
7
|
Protected against the effects of
temporary submersion in water
|
|
|
|
8
|
Protected against the effects of permanent submersion in water
|
|
|
|
9K
|
Protected against water during high pressure/steam cleaning
|
An IP rating, then, combines the solid and liquid rating digits:
-
IP67
—Dust tight, protected from temporary submersion in water
-
IP68
—Dust tight, protected from continuous submersion in water
-
IP69K
—Dust tight, protected from water during high pressure/steam cleaning (but not submersible)
"Solid objects" include a full spectrum from objects larger than 50mm to
minuscule specks of dust. An IP2_ rating indicates that the enclosure will
keep out children's fingers or similar objects; anything smaller than a
finger may get through and do damage. An IP rating of IP6_ designates the
device is dust-tight.
The second digit indicates an enclosure's protection level against liquids.
This designation ranges from 0 to 9K. A rating of 3 means the device is
protected from rain while a rating of 8 shows the case can be submerged for
long periods. A liquid IP designation of _9K indicates the device has the
highest rating indicating it is protected against water during high
pressure/steam cleaning. The caveat is that a _9K rating does not
necessarily mean the enclosure can be submerged (IP_8).
IEC IP Ratings Applied
For those of us who have removed a cover from an electronic enclosure,
whether a computer or an automotive fuse box, dust seems to find a way in.
While low IP solids ratings are focused on keeping the outside world-mainly
your fingers and other probing objects-out of the device, the 5 and 6
designations focus on the ingress of dust into the enclosure. A rating of 5
states dust will not interfere with device operation, while a 6 indicates
no dust or dirt will be present. Desktop computers operate at a level 5 to
balance cooling, cost, and circuit protection requirements. Sensitive
sensors and circuitry often encase or "pot" electronics to prevent any
solids contact and meet an IP6_.
Water can strike an enclosure in many ways. Gravity provides the motive force for vertical impingement often referred to as rain
and dripping. Equipment used outdoors and termed weatherproof generally
align here. Protected receptacles, security cameras, and outdoor lighting
are good examples. When a motive force is added to rain and dripping we have
splashing and spraying. Motive force can occur naturally as in wind or
artificially in an industrial setting like the spray created by coolant in
a machine tool. Finally, when a liquid is pushed through a nozzle, jets are
created. Jets are often used as cleaning applications around the home or in
industrial settings.
We can illustrate the range of liquid IP values using the neighbor's car as
an analogy to an enclosure. The car protects the interior during a
rainstorm (IP_3). If the wind picks up or a passing car hits a puddle
(let's hope his window is up) that is an IP_4. When he washes his car in
his driveway with a hose, that's an IP_5. Finally, going to a commercial
car wash will require an IP_6 rating to keep the interior dry and the
vehicle electronics protected.
Immersion
is a focal point of ingress protection product rating and qualification.
Personal electronic immersion protection was first provided by
wristwatches, then cameras, and most recently cell phones. Here the terms waterproof and water resistant are widely open to
interpretation, but IP67 and IP68 generally bring some clarity. Immersion-proof electronics are found throughout industry from
sensors located within the fluid stream of a processing facility to
communication, sensing and navigation equipment that spend part or all of
their lives submerged in physical bodies of water. The constant-pressure
environments that these enclosures see make proper design, including
redundant sealing systems, necessary
to maximize usable life of the equipment.
High pressure, high temperature wash-down is used throughout industry.
Often, the purpose is to clean microbes and contaminants from equipment
that processes food and pharma. Heavy duty cleaning is required to prepare
machinery for shipment or as part of periodic maintenance. Don't forget the
neighbor who takes a chance at high-temperature pressure washing his engine compartment (hopefully he won't get
even grumpier). Industries where you will find IP69K rating requirements
include food processing, pharmaceutical, petrochemical, waste treatment,
bottling, and transportation.
Mouser Electronics: Harsh Environment Offerings
Mouser offers an entire suite of products meant to handle the abuse of
harsh environments. Ruggedized and sealed enclosures must protect
electronic circuitry from exposure to liquids, particles, and tampering.
Ingress Protection (IP) code (IEC 60529) as well as National Electrical
Manufacturers Association (NEMA) ratings are provided in product data.
To find harsh environment products, use a keyword search (including part
numbers) to search the entire catalog. Alternatively, you can browse by
categories or manufacturers. If you're a registered user, you can use the
note-taking function to aggregate and compile your findings.
Mouser also has a very rich and informative
harsh environments reference section
that provides a wealth of information to assist in specifying and selecting
liquid-tight and dust-tight electronic equipment. Here, you'll find several
thousand electrical enclosures, boxes, cases, racks, and cabinets listed
with corresponding IP values.
The function of the IP code is to provide you with standardized information
about your device's capacity to ward off dust, dirt, and liquids.
Hopefully, it will accurately advise you whether or not your son's iPhone
will take a blast from that grumpy neighbor's water hose.
Steve Schriber, PE is a BSME graduate of Rensselaer Polytechnic Institute. Steve developed a
solid manufacturing foundation working in mechanical and electrical power
transmission, machine tool, and precision instrument industries. He also
ran an engineering consulting company specializing in New York State
chemical bulk storage regulations. This rich experience was a perfect match
for a newly formed internet startup whose mission is to provide a robust
search and discovery experience for engineers and technical buyers. Here he
served in several IC and leadership roles including prime responsibility
for service providers and contract manufacturers. This internet search
engine and content experience provided a broad span of knowledge regarding
many products and services across industries. Leveraging these strengths,
Steve has provided consulting and technical services in the fields of
energy management, manufacturing support, technical writing and content
generation.
In addition to his bachelor's degree, Steve has an MBA from the State
University of New York at Albany. He is a New York State registered
Professional Engineer, an IEP certified Energy Manager, and was certified
as a CPM by in the Institute for Supply Management. He is a member of the
board of directors for the Delta Chapter of Theta Chi at RPI, a Special
Olympics of New York coach and maintains a cross country ski area for the
Town of Greenfield, NY.