Texas Instruments' 16-Bit ADS112C04 ADC, Now at Mouser, Offers Low-Power Conversion for Small Sensor Signals
July 2, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the 16-bit ADS112C04 delta-sigma analog-to-digital converter (ADC) from Texas Instruments (TI). Drawing currents as low was 315 µA, the highly integrated ADS112C04 enables reduced system cost and component count in applications that measure small sensor signals, including resistance temperature detectors (RTDs), thermocouples, thermistors, resistive bridge sensors, and medical monitoring systems.
The TI ADS112C04 ADC, available from Mouser Electronics, features two differential or four single-ended inputs through a flexible input multiplexer (MUX), two programmable excitation current sources, programmable gain amplifier (PGA), a voltage reference, a clock oscillator, and a precision temperature sensor. The device offers two conversion modes — single-shot or continuous — and can perform conversions at data rates up to 2,000 samples-per-second (SPS) with single cycle settling. At 20 SPS, the device's digital filter offers simultaneous 50-Hz and 60-Hz rejection for noisy industrial applications.
The ADS112C04 features a Two Wire, I2C-compatible interface that supports I2C bus speeds up to 1 Mbit per second (Mbps), with two address pins that allow selection of 16 different I2C addresses for the device. The 5.0 mm × 4.40 mm TSSOP device operates from a wide supply range of 2.3 V to 5.5 V over a temperature range of minus 40 to 125 degrees Celsius.
The ADS112C04 ADC is supported by the ADS112C04EVM evaluation module and Delta-Sigma ADC EvaluaTIon Software, which help engineers reduce prototype development time and get products to market faster.
To learn more about the TI ADS112C04 ADC, visit www.mouser.com/ti-ads112c04-adcs.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Trademarks
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com